Adapter for WD Scorpio Black 320GB WD3200BEKT 7200RPM 16MB SATA 2.5" Laptop Hard Disk Drive
Can anyone recommend me that which adapter should I use to read
"WD Scorpio Black 320GB WD3200BEKT 7200RPM 16MB SATA 2.5" Laptop Hard Disk Drive"
as an external drive.
Thanks
Arif
0
Answers
-
Hello @arifakhtar2004 ! Thank you for posting your question.
As that is a SATA drive using the 2.5" form factor with a 9.5mm height, I would recommend the following options:
USB 3.0 - S2510BPU33, S2510BMU33
USB 3.1 - S251BMU313
USB 3.0 (more durable, rugged) - S251BRU33
All of these options include a USB-A cable to connect to your computer. If you prefer connecting via USB-C, an adapter such as our USB31CAADP or cable such as our USB31CUB50CM can be used.
If you have any questions or require any additional assistance, please don't hesitate to reach out!
Jean
0
Categories
- 106 All Categories
- 2 Discover Our Community
- 5 Around the Watercooler
- 21 Idea Station
- 30 Docks, Hubs, Display Adapters
- 5 Mounts, Ergonomics, Desk Accessories
- 11 Networking, Serial, Bluetooth
- 15 Cards, Drive Accessories, Tools
- 5 Racks, Shelves, KVMs
- 11 Cables, AV Splitters, AV Extenders
- 1 Power, Charging