USB Hub for Nitro 5 AN517-41 NH.QAREK.00E
Good day,
I bought the subject laptop and to my surprise it doesn't have video over USB. I'm stuck a bit as I'd like to get a hub that would allow me to use video over USB. The laptop has USB 3.2 I don't have €300 for a hub, so if there isn't anything in the €100-200 range then if someone can suggest just a USB C or A to HDMI converter that would give me video over USB I would appreciate that greatly.
Thanks in advance
Ger
Answers
-
Thanks for your question! Since it appears the USB-C port on that laptop doesn't support DP-Alt mode as you mentioned, the best option is likely a USB-A to HDMI adapter like our USB32HDEH. This adapter requires drivers to be installed and supports up to 1920x1200 resolutions over HDMI.
This adapter features a USB-A hub port, so you don't reduce the total number of USB-A ports available on your laptop. Please also keep in mind USB video adapters like this are not intended for graphics-intensive applications, such as gaming.
2
Categories
- 106 All Categories
- 2 Discover Our Community
- 5 Around the Watercooler
- 21 Idea Station
- 30 Docks, Hubs, Display Adapters
- 5 Mounts, Ergonomics, Desk Accessories
- 11 Networking, Serial, Bluetooth
- 15 Cards, Drive Accessories, Tools
- 5 Racks, Shelves, KVMs
- 11 Cables, AV Splitters, AV Extenders
- 1 Power, Charging