The third model took the settings and is working as expected:
All three devices were purchased from StarTech Store. The third device was purchased at a lower price and has a date code of 2016 and uses a 5V-2A power supply, while the first two duds I tried were newer and had 5V-1A power supplies.
This is the working model:
And these are the previous two models I had purchased:
Date codes. Working model on top:
Model numbers are identical, FCC & IC numbers differ. Working model on right:
Older, working model’s ASIN is B00MZERNXQ, the firmware version from the working printserver is: 9.08.50E 0012 (2015/09/24 21:46:58).
The non-working ASIN is B00M77UME8 and is running firmware 9.08.57E 0017 (2021/03/22 19:32:43)
Is the old firmware available for download so I can attempt to fix my newer device with it?
Thank you!