-
New Here?
Hello! New to the IT Pro Community? First and foremost, welcome! We hope this will be a place where you can learn and engage with your peers on the latest trends in your industry. If you're ready to jump in, but not sure where to start, here are a few tips to help get you on your way: Ask a question, share an idea, or…
-
PM1115UW doesn't hold WiFi settings
I want to connect a printer to the USB port and have it accessible on my existing WiFi, so I'm trying to configure it for Infrastructure WiFi and join it to my existing SSID but when it reboots, it's back in Ad-Hoc mode. This is my second device as StarTec support said since the first one wouldn't hold the configuration,…
-
can not get sound from head phone slot on model ICUSBAUDIO7D.
Hello, I have the following issue with model ICUSBAUDIO7D plug headphone lead into the head phone slot on the device and no sound comes from the speakers, I have download the driver from the startech webpage and have installed the device on windows 10 22H2. Any help to fix this issue would be great. Thank you.
-
SV231DPUCA with a Mac Mini M1
Bonjour, Je souhaite utiliser le commutateur SV231DPUCA, (input en USB-C) avec un mac mini M1 et un mac Studio M1. RIen n'apparait sur l'écran. Le commutateur s'allume dès que je me branche, mais une fois que l'ordinateru 1 est connecté au Commutateur rien ne sepasse. Merci pour votre aide
-
ST121SHD50
Hello, When you are using this HDMI over CAT extender is it needed to use both cables is you are only sending survaillance video and no sound? Or are both cables needed for Power at the receiver side? Or would 2 power supplies fix this issue?
-
How do I get the Startech Thunderbolt 3 to DisplayPort adapter TB32DP14 to work?
How do I get the Startech Thunderbolt 3 to DisplayPort adapter TB32DP14 to work on Microsoft Windows 11 with a Lenovo Thinkpad? It does not see any of the 2 displayport monitors. I tried but it did not work. This adapter seems to be a USB hub and have no video capability even though it is stated to support dual…
-
My Linux and Mac computers don't "see" the real monitor, can the KVM default be changed?
StarTech SV831DUSBU KVM Viewsonic VS11449 monitor (Max resolution 1920 x 1200) But both machines say the monitor is a VGA G56x Linux Mint XFCE 21.1 and Mac OS X 13.6 Both computers support at least 1920 x 1080 and have the latest drivers. Linux box with ATI RV380 video card only lists 1152 x 864 and below Mac box with…
-
KVM issues with Windows and Linux host
I have a SV231TDPU34K, the 3 monitor KVM, that I have connected to a machine that is Windows 10 and a machine that multiboots Windows 11 and various Linux distros. Firstly, if I keep both systems as Windows, the KVM works flawlessly, it switches back and forth with no issue. The issue becomes when I try to use Linux. When…
-
Why is my PC constantly trying to install my USB USB3AAEXT5M active cable?
Everytime I plug in the cable, Windows acts like it is installing the device, but keeps cycling the install so I get that chime sound non-stop. I've already tried pluggin in the cable to other USB ports on the same PC and get the same results.
-
Does the DELL PowerEdge XR12 support the StarTech PCIe card PEX4S232485?
I have questions about the PEX4S232485 (PCI Express card with 2xRS-232 and 2xRS-422/RS-485 ports) cards and whether they will work with the DELL PowerEdge XR12. I have one XR12 with the VMware ESXi 7.0 hypervisor and another XR12 with the Linux OS. For the ESXi system, if I install the PEX4S232485, will I be able to…
-
M.2 SSD SATA Adapter
Hello, I have an SSD M.2 card with the info below. I would like to plug it into a Desktop PC using the SATA interface (I already have a USB adapter). Which SATA / M.2 adapter would work best ? OM3PDP3512B-A01 Digi-Key Part Number: 3217-OM3PDP3512B-A01-ND Manufacturer: Kingston Manufacturer Product Number: OM3PDP3512B-A01…
-
Why would Startech dock DK30CHHPD not work with Dell Vostro 5625 Laptop ?
Hello, we recently purchased DK30CHHPDEU docks to work with our Dell Vostro 5625 (Win11pro) laptops but we have compatibility issues. The dock devices (network, screens and charge) keep disappearing / reappearing every few seconds. We tried 3 different docks on 3 different laptops with the same results. Our laptops have…
-
ACCSMNT Is this CPU mount can be mounted on the wall?
https://www.startech.com/en-eu/display-mounting-ergonomics/accsmnt
-
Power Cable for 4 Port PCI-E USB 3.0 Card
Hello, I bought the 4 port PCI-E USB 3.0 card from StarTech. I absolutely need the optional power connector for my HP G2 VR. Unfortunately, I can't find any instructions on which cable I need for this. I'm not a hardware expert, but there must be a cable that goes from the card (SATA 15 pin female?) directly into the power…
-
under the desk cable management
I would love a no drill under desk cable management tray... something that could hold my power strip and get my cords off the ground, but without having to drill into my desk. Similar to this: Amazon.com: No Drill Under Desk Cable Management Tray, 2 Pack Desk Wire Management Cable Tray Sturdy Alloy Steel Wire Organizer…
-
USB32HD2 causing power surges - can be fixed?
In each USB3 port I try on my computer the USB32HD2 causes a power surge and will not work. Is there a fix?