-
under the desk cable management
I would love a no drill under desk cable management tray... something that could hold my power strip and get my cords off the ground, but without having to drill into my desk. Similar to this: Amazon.com: No Drill Under Desk Cable Management Tray, 2 Pack Desk Wire Management Cable Tray Sturdy Alloy Steel Wire Organizer…
-
Multi-level 5u Rack shelf
I don't know if this is a new idea or is there is more need other than myself however, it's been annoying that I wasted so many R-U space due to small devices. It would be great if a shelf such as this could be made so we don't have devices stack up on top of each other :)
-
(Bring back) Rotating/360 degree USB cables.
Some on the market now that allow full rotation/bending which would be a fantastic feature on our cables. Avoids bending and may help avoid breaking when pulled accidentally. I have an example picture/link - feel free to reach out if this is something worth considering.
-
dock with dual USB-C
Idea from a tech support training today: dock with dual USB-C to exceed 100W charge. Example: Dell Performance Dock – WD19DCS | Dell USA
-
USB3 to USB-C display alt mode
So many USB hubs and touchscreen monitors require USB-C with DisplayPort Alt mode. Not every USB-C port supports DisplayPort alt mode. It should be possible to create a dongle to achieve this. USB 3 to displayport, and USB 3 to a usb hub, internally merged into a usb-C port with display port alt mode
-
8pin GPU female to 15pin Sata male
So, I find myself wanting to power a PCIe expansion card with a Sata or Molex connection on the card. Every computer now has power for two GPUs arriving at the perfect location to place a 6 inch adapter on the second 8-pin and convert it to Sata 15-pin or Molex to power the expansion card ... but can I find an 8-pin female…
-
USB-C / Thunderbolt, external CAD 3D video
In order to properly use CAD/CAM engineering software you need a "workstation graphics" 3D chip, usually either FireGL or Quadro. There has not been a way to do this as an add-on component for laptops without some very complex and expensive custom hardware, to have an internal high-speed video card slot inside a laptop.…
-
Memory card (SD, CFexpress, etc) direct copy/backup to hard drive without computer
Such devices have existed in the past but seem to disappear as soon as the appear in the market. Seems like such a simple thing that is immensely helpful to video and photo professionals or anyone who needs to quickly backup memory card data data to a larger, slower storage medium in the field. Epson made "Multimedia…
-
Add USB-C Power Delivery to MSTCDP123HD
In order to use a 1 USB-C port laptop together with the adapter so it can both charge and display at the same time. I'm using a laptop which has only one USB-C port (Lenovo E15 Gen 2). This port is used for video signal through Thunderbolt 4 and also as power source for charging the laptop. When using MSTCDP123HD it's not…
-
PEX-UB152 Startech needs one of these
Been about 8 years that I have struggled with front panels on my cases that have two Type-C ports but only one header on the motherboard that would support either of those ports. It first started with the Corsair 900D case - now I have purchased the Corsair 1000D case and again with the two USB-C on the front panel but…
-
KVM with Ethernet for sending selections for switching
I recently acquired a SV431DVIUDDM for the purpose of sharing one keyboard and mouse between one laptop and two desktop computers. I can not stress enough how much I love this device. It's so much better than using Synergy or Barrier for the same purpose. USB DDC copy and emulation is the best. One thing that I do miss…
-
Thunderbolt 4 "Switch" 2-4 PC.
I'll be surprised if this hasn't already been suggested but: Overview: A Thunderbolt 4 switch that sits between 2-4 computers (I currently use 3 laptops) and a Thunderbolt 4 Dock. Detail: As with many people, I now find myself working from home. I have all my monitors, keyboard, mouse, misc devices etc connected to a dock.…
-
USB multi computer with individual switches for each port
I have a USB hub that supports two computers and it has 7 USB 2 ports. each individual port has its own switch to connect to either computer. it is a very old USB 2 hub. I would like a USB 3 version that allows each port to also connect to any computer. maybe a 4 computer to several target USB 3 ports.
-
M.2 duplicator
It seems that M.2 SSD duplicators like SSD M.2 PCIe Dock & Duplicator are very interesting product option to add