-
Why is my PC constantly trying to install my USB USB3AAEXT5M active cable?
Everytime I plug in the cable, Windows acts like it is installing the device, but keeps cycling the install so I get that chime sound non-stop. I've already tried pluggin in the cable to other USB ports on the same PC and get the same results.
-
Power Cable for 4 Port PCI-E USB 3.0 Card
Hello, I bought the 4 port PCI-E USB 3.0 card from StarTech. I absolutely need the optional power connector for my HP G2 VR. Unfortunately, I can't find any instructions on which cable I need for this. I'm not a hardware expert, but there must be a cable that goes from the card (SATA 15 pin female?) directly into the power…
-
Best adapter - USB 3.1 to 3440x1440 + Ethernet
Hello there, I'm a little bit lost between all the amazing adapters that you sell. My Laptop has Intel i5-8265U CPU (So with the Intel UHD Graphics 620 GPU), so it can theoretically support a resolution of 4k@60Hz. But in fact no, because Asus equiped it with one HDMI 1.4 port so my new screen with 3440x1440px don't work…
-
The USB to eSATA cables. What chip set is used? Linux blacklists some chips.
Greetings. I am trying to get USB 3's UASP storage mode working on some of my external disk boxes. The Linux kernel blacklists the common JMicron USB 3 to SATA bridge chips, sigh. So, I need to know what chip/chipset you are using in the two cable adapters that go from USB to eSATA, because if they are JMicron, we can save…
-
USB multi computer with individual switches for each port
I have a USB hub that supports two computers and it has 7 USB 2 ports. each individual port has its own switch to connect to either computer. it is a very old USB 2 hub. I would like a USB 3 version that allows each port to also connect to any computer. maybe a 4 computer to several target USB 3 ports.
-
Geekanoids reviews the StarTech Industrial 10-Port USB 3.1 Gen1 Hub HB30A10AME
Dave Cryer AKA @Geekanoids on twitter/youtube posted this unboxing/overview of the Industrial 10-port USB 3.1 Gen 1 Hub on YT. Enjoy!
-
I can't seem to get audio out of my USB32HDES capture card.
My Switch is hooked to the card via HDMI which is then going into my pc's usb 3.0 port. I have the latest drivers for everything, but it's like the Switch isn't outputting audio at all. Neither OBS or my Sound devices window picks up anything from it.