-
Best adapter - USB 3.1 to 3440x1440 + Ethernet
Hello there, I'm a little bit lost between all the amazing adapters that you sell. My Laptop has Intel i5-8265U CPU (So with the Intel UHD Graphics 620 GPU), so it can theoretically support a resolution of 4k@60Hz. But in fact no, because Asus equiped it with one HDMI 1.4 port so my new screen with 3440x1440px don't work…
-
USB3 to USB-C display alt mode
So many USB hubs and touchscreen monitors require USB-C with DisplayPort Alt mode. Not every USB-C port supports DisplayPort alt mode. It should be possible to create a dongle to achieve this. USB 3 to displayport, and USB 3 to a usb hub, internally merged into a usb-C port with display port alt mode
-
USB-C / Thunderbolt, external CAD 3D video
In order to properly use CAD/CAM engineering software you need a "workstation graphics" 3D chip, usually either FireGL or Quadro. There has not been a way to do this as an add-on component for laptops without some very complex and expensive custom hardware, to have an internal high-speed video card slot inside a laptop.…
-
CDP2HDFC - USB-C to HDMIK adapter with Windows 11
Hi All, I've had this adapter for a while and it works fine on another computer. I have one monitor connected the HDMI, and this if for the second one. Both monitors are identical, both react the same way. Both work the way I'd expect on my other laptop. Currently though, I can't get the monitor as an option in Windows.…
-
Add USB-C Power Delivery to MSTCDP123HD
In order to use a 1 USB-C port laptop together with the adapter so it can both charge and display at the same time. I'm using a laptop which has only one USB-C port (Lenovo E15 Gen 2). This port is used for video signal through Thunderbolt 4 and also as power source for charging the laptop. When using MSTCDP123HD it's not…
-
PEX-UB152 Startech needs one of these
Been about 8 years that I have struggled with front panels on my cases that have two Type-C ports but only one header on the motherboard that would support either of those ports. It first started with the Corsair 900D case - now I have purchased the Corsair 1000D case and again with the two USB-C on the front panel but…
-
USB multi computer with individual switches for each port
I have a USB hub that supports two computers and it has 7 USB 2 ports. each individual port has its own switch to connect to either computer. it is a very old USB 2 hub. I would like a USB 3 version that allows each port to also connect to any computer. maybe a 4 computer to several target USB 3 ports.
-
New Blog Post! "How Using the Right USB-C Multiport Adapter Can Boost Productivity"
Hey Community Friends! We've just published a new blog post discussing our various USB-C Multiport Adapters. We focus on how selecting the right one can boost your productivity. Check it out, and don't forget to download a copy of our Multiport Adapter grid to check out the full selection of adapters. What features are…
-
NEW POST: Meet Our High Performance USB-C Cables
Another new blog post about cables is live! We welcome your comments and feedback. Have you found the perfect application for these new performance-focused USB-C cables?
-
NEW POST: Essential IT Accessories for the Home Office
Please check out our latest blog post at the link below, and then comment on this thread to let us know if you have any great accessory suggestions!
-
NEW POST: Cables That Deliver Performance
Please check out our new blog post at the link below, and then comment here if you have any questions about the best performance cable to choose for your rigorous application.
-
Best wall charger for Pixel 6?
What's the best wall charger to use with a Pixel 6? I'm looking to maximize the charge rate, and get results similar to the OEM charger at a second location.