Why is the power LED on USB4PACxx slowly blinking? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>This device provides 6.8A of power, and the power LED on the device will slowly blink when the devices connected to it are trying to draw more than 6.8A of power. To properly charge the connected devices, reduce the number or types of devices connected to this device until the power LED stops blinking.</p><p><br></p><p><br></p><div class="blockquote"><div class="blockquote-content"><p class="blockquote-line">This FAQ applies to these products:</p><p class="blockquote-line"><a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fcables%2Fusb4pacbk" rel="nofollow noreferrer ugc">USB4PACBK</a> <a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fcables%2Fusb4pacwh" rel="nofollow noreferrer ugc">USB4PACWH</a></p></div></div><p><br></p> </article> </main>