Will TBT3TBTADAP pass through the full wattage of bus power from the host Thunderbolt 3 port? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>No, this device will not pass through the full wattage of bus power from the host Thunderbolt 3 port. This adapter uses up to 4.5W of power, which prevents devices that require the full wattage of bus power from working.</p> </article> </main>