What factors impact the performance of the SDOCK1EU3P? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>The suggested time that the erase process will take is a conservative estimate based on the characteristics of the individual hard drive, including the maximum read and write speeds and overall health of the hard drive. The erase mode that you select can also impact the time it takes to erase the drive, as the more in-depth erase modes require more resources.</p> </article> </main>