How can I tell which M.2 hard drives will work in PEX4M2E1 or PEX4SFF8643 ? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>Although M.2 SSDs come in similar form factors, only an M.2 PCIe drive with an M.2 NGFF M key will operate with this device. M.2 drives that are SATA or drives that have a different key position are not compatible with this device.</p><p>This device can adapt an M.2 PCIe drive to connect to PCIe connections, which is not possible for a SATA based M.2 drive. The key type refers to the connector type on the M.2 PCIe drive, and the M key can only be M.2 PCIe. It is important to check the specifications of the drive to see if it supports PCIe M key.</p><p><br></p><p><br></p><div class="blockquote"><div class="blockquote-content"><p class="blockquote-line">This FAQ applies to these products:</p><p class="blockquote-line"><a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fhdd%2Fpex4m2e1" rel="nofollow noreferrer ugc">PEX4M2E1</a></p><p class="blockquote-line"><a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fhdd%2Fpex4sff8643" rel="nofollow noreferrer ugc">PEX4SFF8643</a></p></div></div><p><br></p> </article> </main>