The fault LED is on but the POEINJ1G1 is working. What do I do? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>If an extra power source is not connected to either the PWR1 or PWR2 terminal blocks on the POEINJ1G1, the fault LED lights up, regardless of whether or not the unit is working properly. The fault LED is lit up because the POEINJ1GI does not detect a redundant power source. To avoid the fault LED being lit up, connect a power source to both PWR1 and PWR2.</p> </article> </main>