How do I need to format my hard drive for the S2510BU3ISO ISO function to work? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>To use the S2510BU3ISO to load ISO images, the drive must have the following parameters:</p><ul><li>Non-Advance Format drive (512 byte sector size, not 4k).</li><li>Boot Sector: Master Boot Record (MBR).</li><li>Partion: NTFS.</li><li>Sector Size: Default Sector Size.</li></ul><p>If the enclosure is not formatted with these parameters, it will not lock on to an ISO (located in an <strong>_iso</strong> folder) and will only function as an external mass storage device.</p> </article> </main>