Will PEX4M2E1 / PEX4SFF8643 allow me to boot an operating system from my hard drive? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>You can use this hard drive adapter to boot an operating system from; however, depending on the SSD and motherboard that you are using, you may need to update the driver or BIOS in order for the hard drive to be seen when you initially boot the operating system.</p><p>If you experience issues when you use the hard drive adapter to boot an operating system, check with the manufacturers of the SSD and motherboard for updates.</p><p>You should also check to make sure that the SSD and motherboard are compatible. For more information, refer to the following FAQ: <a href="https://community.startech.com/kb/articles/109-are-there-any-hard-drives-or-motherboards-that-are-incompatible-with-pex4m2e1-or-pex4sff8643" rel="nofollow noreferrer ugc">Are there any hard drives or motherboards that are incompatible with PEX4M2E1 or PEX4SFF8643 ? - StarTech.com IT Pro Community</a></p> </article> </main>