Can I use USB flash drive duplicators with external hard drive enclosures? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>Although the USB flash drive duplicators are intended for use with USB flash drives, they can be used with external hard drives.</p><p><strong>Note:</strong> Due to the slower copy speed of the USB flash drive enclosures, using an external hard drive as the source of the copy can take a considerable amount of time. USBDUP12 and USBDUP15 both copy at 1.5 GB per minute. Therefore, if you use a 1 TB external hard drive as the source of a copy, it would take roughly 11 hours to complete.</p><p><br></p><p><br></p><div class="blockquote"><div class="blockquote-content"><p class="blockquote-line">This FAQ applies to these products:</p><p class="blockquote-line"><a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fhdd%2Fusbdup12" rel="nofollow noreferrer ugc">USBDUP12</a> <a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fhdd%2Fusbdup15" rel="nofollow noreferrer ugc">USBDUP15</a></p></div></div><p><br></p> </article> </main>