Can I capture the output of my USB2HDCAPS on multiple computers? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>A single USB2HDCAPS can stream over the network to multiple systems simultaneously. This allows multiple systems running ShareView to view or record the input to the USB2HDCAPS.</p><p>Multiple USB2HDCAPS can also exist on the network and can be selected in the ShareView <strong>Settings</strong> menu.</p><p>Only the first system that is connected to the USB2HDCAPS can change the settings; other systems that are connected to the unit can only view and record the video data.</p><p><strong>Note:</strong> While third-party software may work with the USB2HDCAPS, StarTech.com only supports the use of ShareView software for network streaming.</p> </article> </main>