Are there any network requirements for the USB2HDCAPS? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>In order for network streaming to work with ShareView, your network infrastructure must have a DHCP server included on the network. The DHCP server issues an IP address to the USB2HDCAPS and allows any computer on the same network running ShareView to discover the USB2HDCAPS.</p><p>When you use network streaming with the USB2HDCAPS, consider the following:</p><ul><li>A static IP address cannot be set.</li><li>Only a 10/100 connection is required.</li><li>StarTech.com only supports the use of ShareView software for network streaming and does not support the use of third-party streaming software.</li></ul> </article> </main>