Does TB4CDOCK support monitor resolutions greater than 4K and are adapters required? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>Yes, when connected to a host that also supports these higher resolutions, the<em> </em>TB4CDOCK can support <strong>dual monitors</strong> with resolutions <strong>up to 4K 60Hz</strong>, or a <strong>single monitor</strong> with resolutions <strong>up to 8K 30Hz</strong>, 6K 60Hz, 5K 60Hz. Depending on the video port on the monitor, supported adapter/cables like these may also be required and are not included with the dock. Monitor connection:</p><ul><li>USB-C: USB31CCV1M</li><li>DisplayPort: CDP2DP141MB</li><li>HDMI: CDP2HDMM1MH</li><li>DVI: CDP2DVIMM1MB</li><li>VGA: CDP2VGAMM1MB </li></ul><div class="embedExternal embedImage display-large float-none"> <div class="embedExternal-content"> <a class="embedImage-link" href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fus.v-cdn.net%2F6035386%2Fuploads%2FCW71JQ96A06T%2Fimage.png" rel="nofollow noreferrer noopener ugc" target="_blank"> <img class="embedImage-img" src="https://us.v-cdn.net/6035386/uploads/CW71JQ96A06T/image.png" alt="image.png" height="2000" width="2000" loading="lazy" data-display-size="large" data-float="none"></img></a> </div> </div> <p>Note: the TB4CDOCK is not currently supported on Windows-based <strong>Thunderbolt 3</strong> hosts.</p> </article> </main>