What are some ideal accessories for a Thunderbolt 4 dock? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>The multiple TB4 hub ports allow plenty of flexibility with the TB4CDOCK. Here are some examples of adapters that allow connecting a variety of devices quickly and easily to the USB-C hub ports on the dock. Keep in mind these ports on the dock will be limited by the capability of the host computer (e.g. connecting the dock to a Thunderbolt 3 host port will <em>not allow</em> the dock’s hub ports to operate as full Thunderbolt 4 ports).</p><ul><li>DisplayPort Display: CDP2DP141MB</li><li>HDMI Display: CDP2HDMM1MH</li><li>USB-A Device: USB31CAADP</li><li>USB-C Device: USB-C: USB31CCV1M </li></ul><p><br></p> </article> </main>