How do I install PM1115U2 in Windows using the software? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>To add a printer from the print server to your Windows computer, you need to use the provided software to locate the print server on your network.</p><h3 data-id="hardware-requirements">Hardware requirements</h3><ul><li>A wired Ethernet network with DHCP (automatically assigned IP addresses).</li><li>A compatible USB printer.</li><li>A computer running Windows.</li></ul><h3 data-id="install-the-hardware">Install the hardware</h3><ol><li>Use a USB A-to-B cable to connect the USB printer to the PM1115U2.</li><li>Use an Ethernet patch cable to connect the PM1115U2 to a wired Ethernet network (for example, a network switch, wall jack, and so on).</li><li>Connect a power supply to the print server.</li></ol><h3 data-id="install-the-software">Install the software</h3><ol><li>Navigate to <a href="https://community.startech.com/home/leaving?allowTrusted=1&target=http%3A%2F%2Fwww.startech.com%2FSupport" rel="nofollow noreferrer ugc">http://www.startech.com/Support</a> and download the latest software. You can find the part number and product ID on the product packaging.</li></ol><p><strong>Note:</strong> Windows typically saves the files to the <strong>Downloads</strong> folder that is associated with your user account (for example, C:\Users\<em>your_name</em>\Downloads).</p><ol><li>When the download is complete, right-click the zip folder that you downloaded, click <strong>Extract All</strong>, and follow the on-screen instructions.</li><li>In the list of extracted files, right-click the <strong>Network Printer Wizard Setup 2017 with Window 8.exe </strong>file and click<strong> Run as Administrator</strong>.</li><li>Follow the on-screen instructions to install the driver software.</li></ol><h3 data-id="configure-the-software">Configure the software</h3><p>After the Network Printer Wizard is installed on your system you can install the printer. To install the printer, complete the following:</p><ol><li>Open the <strong>Launch Network Printer Wizard</strong>.</li><li>Click <strong>Next.</strong></li><li>Select the print server from the list and click <strong>Next</strong>.</li><li>Select the appropriate driver for the printer and click <strong>Next</strong>. If you cannot find the driver, use a generic PCL5/PCL6/PS driver or obtain the driver from the manufacturer of your printer.</li><li>Click <strong>Finish.</strong></li></ol><h3 data-id="verify-the-installation">Verify the installation</h3><ol><li>Open <strong>Control Panel</strong>.</li><li>Navigate to <strong>Devices and Printers</strong> or <strong>Printers and Other Hardware.</strong></li><li>Right-click the installed printer and click <strong>Printer Properties.</strong></li><li>Click <strong>Print Test Page.</strong></li></ol><p>A printer test page should be sent to your printer.</p> </article> </main>