I have a charging icon while the TB3DKDPMAW is plugged in, but my system is not charging. What do I do? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>This docking station provides 15 watts of power, which may be enough to display a charging icon, but is likely not enough to restore battery power while the system is on and being used. If an icon is displayed and the system is put into sleep mode, battery power will be restored slowly.</p><p><br></p><div class="blockquote"><div class="blockquote-content"><p class="blockquote-line">This FAQ applies to these products:</p><p class="blockquote-line"><a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fhdd%2Fbndtb4m2e1" rel="nofollow noreferrer ugc">BNDTB4M2E1</a> <a href="https://community.startech.com/home/leaving?allowTrusted=1&target=https%3A%2F%2Fwww.startech.com%2Fen-us%2Fcards-adapters%2Ftb3dkdpmaw" rel="nofollow noreferrer ugc">TB3DKDPMAW</a></p></div></div><p><br></p> </article> </main>