How do I access the PM1115U2 web interface? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>To determine the IP address of the PM1115U2, do one of the following:</p><ul><li>Use the Windows Network Printer Wizard to determine the IP address.</li><li>View the router's DHCP table to determine the IP address. The print server should be listed with a MAC address starting with 80:3F:5D.</li></ul><p> To access the print server web interface, complete the following:</p><ol><li>Make sure that the computer is on the same network as the PM1115U2. </li><li>In an Internet browser, enter the IP address of the PM1115U2.</li><li>Click <strong>Login</strong>. </li></ol><p><br></p> </article> </main>