How do I set up PM1115U2 without using the provided software? - StarTech.com IT Pro Community
<main> <article class="userContent"> <p>If you are using applications that do not support print server software, you can use the web interface to configure the print server for your network. To access the web interface you need to determine the IP address of the PM1115U2. This device has Dynamic Host Configuration Protocol (DHCP) enabled by default, and will be assigned an IP address by your router when connected to your network. </p><p>You can determine the IP address of the unit in one of the following ways:</p><ul><li>Use the Windows Network Printer Wizard to determine the IP address.</li><li>View the router's DHCP table to determine the IP address. The print server should be listed with a MAC address starting with 80:3F:5D.</li></ul><p>To access the print server web interface, complete the following:</p><ol><li>Make sure that the PM1115U2 is on the same network as your computer.</li><li>In an Internet browser, enter the IP address of the unit.</li><li>Click <strong>Login</strong>.</li></ol><p>You can now access the print server configuration and make the necessary changes for it to work on your network.</p> </article> </main>