-
What port should be selected when using the ICUSB128410 in Windows?
Once installed, the ICUSB128410 will show up as a virtual port: USB001 To use this virtual port with a printer, follow these steps: Ensure the printer drivers from the printer manufacturerhave been installed.Open Control Panel > View devices and printers.Find the entry for the printer.Right-click the printer and choose…
-
Power over Ethernet (PoE) Explained
Overview Power over Ethernet (PoE) allows power to be carried over network cables. PoE devices are divided into two categories: Power Sourcing Equipment (PSE) are devices that supply power over Ethernet cables. Examples are PoE Switches, PoE Network Cards, PoE Injectors, and PoE Fiber Media Converters. Powered Devices (PD)…
-
Are there any limitations to using DisplayLink products with my Android device as the host?
Despite the stated maximum resolution and number of displays for this product, it is currently limited to connecting a single display at 1920x1080 through the DisplayLink chipset when using an Android device as the host system. This is a limitation which affects all DisplayLink powered products, regardless of manufacturer,…
-
How do I choose a VESA mount for my display?
VESA (Video Electronics Standards Association) mounting standards define the mounting hole patterns on the back of displays. For example: 100x100, 200x300, 300x300. Ensure the mount you choose includes compatibility for the size and the spacing of the mounting holes on the back of your display. Not all displays or mounts…
-
What are the two modes on the DK31C3MNCR dock?
Modes Four lane mode (default) - Features 4K video performance with USB 2.0 480Mbps throughput Two lane mode - Features 1080p video performance with USB 3.2 Gen2 10Gbps throughput How to Switch Modes Hold power button for 4 sec to switch between two and four lane modes. Status LED Solid Green LED = Dock is powered on in…
-
How do I install PM1115U2 in Windows using the software?
To add a printer from the print server to your Windows computer, you need to use the provided software to locate the print server on your network. Hardware requirements A wired Ethernet network with DHCP (automatically assigned IP addresses). A compatible USB printer. A computer running Windows. Install the hardware Use a…
-
Where can I find product Compliance and Safety documents?
This article was created from information and screenshots by Federico G. Available product compliance and safety documentation like RoHS, REACH, WEEE (Waste Electrical and Electronic Equipment Directive), COO (Country of Origin), DOC (Declaration of Conformity) can be downloaded from the product page on our website. Enter…
-
Why is DK31C3HDPD Video 1 output not working with my Mac computer?
On the early original revision of DK31C3HDPD, Video 1 ports (HDMI and DP) don't work when connected to some models of Mac. This limits the dock to 2x external displays, on Video 2 and Video 3 ports. Affected Models Apple M1 Processor Mac mini (2020) MacBook Pro (13-inch, 2020) MacBook Air (2020) Intel Processor MacBook Air…
-
What is the main difference between HDMI cable types, and are they backward compatible?
This article was created from a community discussion by luil. HDMI 2.1 - Certified Ultra High Speed HDMI Cable Ultra High Speed HDMI 2.1 Certification ensures that cables like our HDMM21V2M will deliver full 8K performance & beyond. This line of cables are also encased in die-cast aluminium shielding to improve signal…
-
What is USB-C Power Delivery (PD) pass-through?
This article was created from a community discussion by jtan. Using Power Delivery pass-through with a supported USB-C laptop, you can power the laptop and the multiport adapter/hub with your existing USB-C laptop power adapter. To ensure the hub powers and charges your laptop, your host laptop's USB-C port must support…