-
What port should be selected when using the ICUSB128410 in Windows?
Once installed, the ICUSB128410 will show up as a virtual port: USB001 To use this virtual port with a printer, follow these steps: Ensure the printer drivers from the printer manufacturerhave been installed.Open Control Panel > View devices and printers.Find the entry for the printer.Right-click the printer and choose…
-
Power over Ethernet (PoE) Explained
Overview Power over Ethernet (PoE) allows power to be carried over network cables. PoE devices are divided into two categories: Power Sourcing Equipment (PSE) are devices that supply power over Ethernet cables. Examples are PoE Switches, PoE Network Cards, PoE Injectors, and PoE Fiber Media Converters. Powered Devices (PD)…
-
How do I install PM1115U2 in Windows using the software?
To add a printer from the print server to your Windows computer, you need to use the provided software to locate the print server on your network. Hardware requirements A wired Ethernet network with DHCP (automatically assigned IP addresses). A compatible USB printer. A computer running Windows. Install the hardware Use a…
-
With PM1115U2 in Windows, how do I add the printer to my computer from my print server?
In Windows 10, to add a printer to your computer, you need to create a print server port. Before you create the print server port, you need to configure your print server for the network. For more information about how to configure your print server, refer to the following FAQ: To create a print server port, complete the…
-
USB56KEMH2 Fax Modem Windows 10 Setup Guide
This guide shows how drivers look from auto-install vs. StarTech.com drivers, how to set up the modem in Windows Fax and Scan, how the adapter should appear and react, and the steps to test basic functionality on a fax/phone line. 1. After being plugged in the first time the fax modem will auto-install the generic…
-
How do I install PM1115UW on Windows or macOS?
Manual Setup & Install on Windows and macOS This video walks you through how to manually set up PM1115UW in Windows or macOS. There is also a Manual Setup & Install Guide in PDF format available. Software-guided Install on Windows Only 1. With an Ethernet cable connect the print server to an available Ethernet port on the…