-
How can drive compatibility be increased on IDE2SAT2?
ACD Jumper stands for ATAPI CD-ROM. IDE2SAT2 doesn’t typically require the ACD jumper for use with optical drives and you should be able to use the cable select jumper position on this adapter instead. That being said, the ACD jumper is specifically for increasing optical drive compatibility, so if it doesn’t work in cable…
-
How do I power off the S352BU313R enclosure?
To power down the S352BU313R, follow these steps: Ensure both blue drive activity LEDs on the front of the unit are off (indicating no drive read/write activity). Power off the enclosure using the power switch on the back of the unit.
-
S352BU313R - RAID Configuration
This article was created from a community discussion by agzol and internal testing by JustinW. Follow these steps to configure drives in RAID on S352BU313R enclosure: Move the Power switch on the dual-bay enclosure to the OFF position. Use a Philips screwdriver to remove the four screws in the back panel. Remove the drive…
-
What is PCIe Bifurcation?
This article was created from a community discussion by @JustinW. PCIe bifurcation is a feature that allows the division of data lanes in a PCIe slot. For instance, on supported systems a PCIe x16 slot can be configured into two PCIe x8 lanes, or more smaller lanes, depending on what the motherboard supports. PCIe…
-
How do I know if a RAID1-configured drive has failed in the 25S22M2NGFFR?
Identifying Failed Drive If you have two drives configured in a RAID1 array, and one of the drives fails, the remaining drive will still show in the OS, but you will be unable to access it (no read/write). You would then need to remove the cover from the 25S22M2NGFFR and power on the enclosure to observe the internal LEDs.…
-
What is the input/output specifications on ICUSBAUDIO?
The output voltage is 1.25V RMS typical, with a +0.5V to +4.0V swing The input range is 0V pp to 2.88V pp (volts peak to peak). Please note these adapters have a mic-level input and not a line-level input. This FAQ applies to these products: ICUSBAUDIO ICUSBAUDIOB
-
How do I initialize a brand new hard drive in Windows or macOS?
Windows 10 Before you can access a new or formatted drive in your operating system, you need to initialize it first and then create a partition on the drive. A partition defines an area of the drive to use for storing data. The partition uses a file system (for example, ex-FAT, NTFS, and so on). Initialize a driveNote: You…
-
Do video capture devices work with DirectShow?
The specific video capture devices listed in this bulleted list use a DirectShow compatible driver and can be used with many third-party video capture applications that are compatible with DirectShow: ECHDCAP PEXHDCAP PEXHDCAP60L USB32DVCAPRO USB32HDCAPRO USB32VGCAPRO USB3HDCAP UVCHDCAP The driver for your video capture…
-
How do I need to format my hard drive for the S2510BU3ISO ISO function to work?
To use the S2510BU3ISO to load ISO images, the drive must have the following parameters: Non-Advance Format drive (512 byte sector size, not 4k). Boot Sector: Master Boot Record (MBR). Partion: NTFS. Sector Size: Default Sector Size. If the enclosure is not formatted with these parameters, it will not lock on to an ISO…