-
How can drive compatibility be increased on IDE2SAT2?
ACD Jumper stands for ATAPI CD-ROM. IDE2SAT2 doesn’t typically require the ACD jumper for use with optical drives and you should be able to use the cable select jumper position on this adapter instead. That being said, the ACD jumper is specifically for increasing optical drive compatibility, so if it doesn’t work in cable…
-
How do I power off the S352BU313R enclosure?
To power down the S352BU313R, follow these steps: Ensure both blue drive activity LEDs on the front of the unit are off (indicating no drive read/write activity). Power off the enclosure using the power switch on the back of the unit.
-
S352BU313R - RAID Configuration
This article was created from a community discussion by agzol and internal testing by JustinW. Follow these steps to configure drives in RAID on S352BU313R enclosure: Move the Power switch on the dual-bay enclosure to the OFF position. Use a Philips screwdriver to remove the four screws in the back panel. Remove the drive…
-
How do I know if a RAID1-configured drive has failed in the 25S22M2NGFFR?
Identifying Failed Drive If you have two drives configured in a RAID1 array, and one of the drives fails, the remaining drive will still show in the OS, but you will be unable to access it (no read/write). You would then need to remove the cover from the 25S22M2NGFFR and power on the enclosure to observe the internal LEDs.…
-
How do I need to format my hard drive for the S2510BU3ISO ISO function to work?
To use the S2510BU3ISO to load ISO images, the drive must have the following parameters: Non-Advance Format drive (512 byte sector size, not 4k). Boot Sector: Master Boot Record (MBR). Partion: NTFS. Sector Size: Default Sector Size. If the enclosure is not formatted with these parameters, it will not lock on to an ISO…