# Article: How to choose the right KVM?

**URL:** https://community.startech.com/t/article-how-to-choose-the-right-kvm/1688
**Category:** Racks, Shelves, KVMs
**Created:** [June 23, 2025, 5:39pm UTC](https://community.startech.com/t/article-how-to-choose-the-right-kvm/1688 "2025-06-23T17:39:25Z")
**Posts on this page:** 1
**Page:** 1

<div class="post-metadata">

### Author: ![EmmanuelB](https://yyz2.discourse-cdn.com/flex012/user_avatar/community.startech.com/emmanuelb/32/24_2.png) [@EmmanuelB](https://community.startech.com/u/EmmanuelB)
#### Post date: [June 23, 2025, 5:39pm UTC](https://community.startech.com/t/article-how-to-choose-the-right-kvm/1688/1 "2025-06-23T17:39:25Z")

</div>

### How to choose the Right KVM?

A KVM (Keyboard, Video, Mouse) switch is a device that allows you to control multiple computers using a single keyboard, monitor, and mouse setup. This can be incredibly useful for those who need to manage several computers from one desk, making it easier to switch between systems without the need for multiple peripherals.

#### Preparing the Right Questions

When choosing the right KVM switch, it’s essential to ask yourself a few key questions to ensure you select the best option for your needs:

1. **How many computers will you be connecting?**

- Determine the number of computers you need to control. This will help you decide how many ports your KVM switch should have.

1. **How many monitors will you be using?**

- Consider the number of monitors you plan to connect. Some KVM switches support multiple monitors, which can be crucial for users who require a multi-display setup.

1. **What type of inputs do your monitors support?**

- Check the input types (HDMI, DisplayPort, DVI or VGA) that your monitors support. This will help you choose a KVM switch that is compatible with your existing hardware.

#### Adjusting for Different Ports

If one of your computers does not have the same ports or does not have enough ports, there are solutions available:

- **Using another port and converting it:** You can use adapters to convert one type of port to another. For example, if your KVM switch uses HDMI but one of your computers only has DisplayPort, you can use a DisplayPort to HDMI adapter.
- **Adding a new video port using USB Video Technology:** If your computer lacks the necessary video ports, you can add new ones using USB video adapters. These adapters allow you to add additional video outputs via USB, making it easier to connect to your KVM switch.

#### Types of KVMs

There are different types of KVM switches available, each catering to specific needs:

- **Standard Box Types:** These are simple boxes with all the necessary cables provided separately. They are versatile and can be used in various setups.
- **Compact Cable Types:** These KVM switches come with embedded cables, making them a more straightforward solution for those who prefer a clutter-free setup.
- **Docking Station-Based KVMs:** These are docking stations that allow connection to two hosts and switching between them. They are ideal for users who need a more integrated solution with additional connectivity options.

#### Conclusion

To find the proper KVM switch for your needs, start by laying down the number of computers and monitors you need to connect. This will help you determine the right type of KVM switch. If you require any assistance in finding or installing a KVM switch, please contact our [support team](https://www.startech.com/support).