I am using the TB31PCIEX16 under Ubuntu 24.04 with a fire wire card from StarTech.
All works fine.
Only the fan of the case is quite disturbing. What are the technical specifications of this fan so that I can replace it e.g. with a corresponding and more silent fan from Noctua?
Other possibility would be some StarTech software to switch the fan off if e.g. the temperature is low in the case (the firewire card does not produce that much heat I guess).
The enclosure’s fan speed cannot be disabled or adjusted through software. However, the fan can be replaced with a compatible 60x10mm fan featuring a TX3 connector, such as the StarTech.com FAN6X1TX3.
Noctua NF-A6x15 FLX
Slim 60x15mm premium fan
12 V
0.085 A input current
would also be possible since the StarTech FAN6X1TX3 needs 160mA?
Startech is: 15.49 CFM, 28 dBA and 4000 RPM
Noctua is: 23.4 m³/h (13.77 CFM),19.8 dB(A), 3500 rpm
The original fan is a
RUNDA RS6015S12L
60 × 60 × 15 mm
60mA