# SVID2USB232 – The signal turns black and white after a few seconds

**URL:** <https://community.startech.com/t/svid2usb232-the-signal-turns-black-and-white-after-a-few-seconds/1774>\
**Category:** Cards, Drive Accessories, Tools\
**Tags:** usb\
**Created:** [August 10, 2025, 9:16pm UTC](https://community.startech.com/t/svid2usb232-the-signal-turns-black-and-white-after-a-few-seconds/1774 "2025-08-10T21:16:11Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![Linkar](https://avatars.discourse-cdn.com/v4/letter/l/f17d59/32.png) [@Linkar](https://community.startech.com/u/Linkar)\
**Post date:** [August 10, 2025, 9:16pm UTC](https://community.startech.com/t/svid2usb232-the-signal-turns-black-and-white-after-a-few-seconds/1774/1 "2025-08-10T21:16:11Z")

</div>

Greetings,

I regularly use a Startech SVID2USB232 card and OBS to digitize family VHS tapes or those belonging to my friends and acquaintances.

I have a simple setup with a VCR that outputs a Peritel signal, which I pick up via RCA and/or S-video. The signal goes into a Startech SVID2USB232 card that I plug into USB, and it shows up as a video source in OBS.

I’ve never had any problems with this setup. The last time I digitized VHS tapes was two months ago, and everything worked fine.

I recently received some new tapes and encountered a problem that I don’t understand. It’s very simple: after a few seconds, the signal that was appearing correctly switches to black and white. As soon as I reset one of the capture settings, the color returns, then disappears after 5-6 seconds.

I made a video to show you the problem: [https://youtu.be/rFynInU8mmA](https://youtu.be/rFynInU8mmA)

!! I should mention that I’m French, so the VHS format I use is SECAM !!

This problem doesn’t occur with all the tapes, only some of them are interpreted this way.

I am posting this today because I have conducted several tests that lead me to believe that the SVID2USB232 is the problem. I have tested several capture software programs and several versions of these programs (OBS, Movavi, etc.), and the result is always the same. I tried changing the setup by shortening the cables as much as possible to increase the signal strength, but that didn’t change anything. I reinstalled the drivers and also tried older versions, but that didn’t change anything either. I connected the VCR directly to a monitor and the VHS plays correctly with the right colors, so the signal coming out of the VCR is fine.

I’m starting to think that it’s the Startech card that is misinterpreting the signal sent to it…

Thank you in advance if you can provide me with a solution.

Version française :

Bonjour,

J’utilise régulièrement une carte Startech SVID2USB232 et OBS pour numériser des VHS familiales ou celles des familles de mes amis et connaissances.

J’ai un setup simple avec un magnétoscope qui sort un signal en Peritel que je reprends en RCA et/ou S-video, le signal arrive dans une carte Startech SVID2USB232 que je branche en USB et qui apparait comme une source vidéo dans OBS.

Je n’ai jamais eu de problèmes avec ce setup, la dernière fois que j’ai numérisé des VHS c’était il y a 2 mois et tout allait bien.

J’ai reçu de nouvelles cassettes il y a peu et j’ai rencontré un problème que je ne comprends pas. C’est très simple, au bout de quelques secondes le signal qui apparaissait correctement passe en noir et blanc. Dès que je réinitialise un des paramètres de capture, la couleur revient puis elle disparait au bout de 5-6 secondes.

Je vous ai fait une vidéo pour vous montrer le problème : [https://youtu.be/rFynInU8mmA](https://youtu.be/rFynInU8mmA)

!! Je précise que je suis français, le format VHS chez moi c’est du SECAM !!

Ce problème ne se présente pas avec toutes les casettes, seulement certaines sont interprétées de la sorte.

Je dépose ce post aujourd’hui car j’ai mené plusieurs tests qui me laisse à penser que c’est la SVID2USB232 qui pose problème. J’ai testé plusieurs logiciels de capture, et plusieurs versions de ces logiciels (OBS, Movavi, …) le résultat est toujours le même. J’ai essayé de changer le setup en raccourcissant au maximum la longueur des câbles afin d’augmenter la force du signal, ça n’a rien changer. J’ai réinstallé les drivers et également tenté avec d’anciennes versions, ça ne change rien. J’ai branché le magnétoscope directement sur un écran et la VHS est lue correctement avec les bonnes couleurs, donc le signal qui sort du magnétoscope est bon.

J’en arrive à penser que c’est la carte Startech qui interprète mal le signal qui lui est envoyé…

Merci d’avance si vous pouvez m’apporter une solution.

---

<div class="post-metadata">

**Author:** ![EmmanuelB](https://yyz2.discourse-cdn.com/flex012/user_avatar/community.startech.com/emmanuelb/32/24_2.png) [@EmmanuelB](https://community.startech.com/u/EmmanuelB)\
**Post date:** [August 11, 2025, 7:56pm UTC](https://community.startech.com/t/svid2usb232-the-signal-turns-black-and-white-after-a-few-seconds/1774/3 "2025-08-11T19:56:17Z")

</div>

Hello @Linkar and thank you for your interest in our Community.

For situations like this, the best way to isolate the issue is to test the following:

- Test with different media (different records, different tapes).
- Test with different video source (a different device with composite or S-Video output).
- Test with different capture software (Movavi, OBS, VLC).
- Make sure to be running the latest drivers directly from our web site (Default, non-TWAIN).
- Test on a different computer.

From my understanding, you’ve already confirmed most of these items: I’d recommend making sure to be running on the [latest drivers](https://www.startech.com/fr/SVID2USB232) (default, non-TWAIN) as well as testing on a different computer.

Ultimately, if these steps do not either solve or isolate the source of the issue, the next step would be to contact our [Technical Support](https://www.startech.com/fr/support) (ideally by chat or phone), preferably while in front of the setup in question. This will allow us to perform some live test with you and potentially proceed with a replacement if the item is indeed deemed defective.

I hope this helps!

Emmanuel B.  
[StarTech.com](http://StarTech.com) Support