Article: What are some ideal accessories for a Thunderbolt 4 dock?

The multiple TB4 hub ports allow plenty of flexibility with the TB4CDOCK. Here are some examples of adapters that allow connecting a variety of devices quickly and easily to the USB-C hub ports on the dock. Keep in mind these ports on the dock will be limited by the capability of the host computer (e.g. connecting the dock to a Thunderbolt 3 host port will not allow the dock’s hub ports to operate as full Thunderbolt 4 ports).

  • DisplayPort Display: CDP2DP141MB
  • HDMI Display: CDP2HDMM1MH
  • USB-A Device: USB31CAADP
  • USB-C Device: USB-C: USB31CCV1M