WASD is no more, sadly.
But, the DIP switch settings are set to be a completely HID device (no extra functionality enabled, like rollover keys, etc) - works on all other HID type ports.
As to the Linux computer:
- The make is an MSI Mag B650 Tomahawk Wifi motherboard, and I’ve tried the following connections:
- Connected the USB-C to USB-B port to the USB-C port on * this front port assembly, which is connected to the JUSB1 jumper on the motherboard, which is a USB 3.2 Gen 2 Type-C Connector. This should have PLENTY of power.
- Connected the USB-A to USB-B cable to a case provided USB port that connects to the JUSB3 USB 2.0 header.
- In all cases, no errors regarding USB connections in dmesg - I’ll try connecting the keyboard to the HID port again, just to see if there’s an error, nor simply no message at all when I plug it in.
Oh, and the HID ports don’t work for either the Mac or the Linux systems connected.