Article: How do I initialize a brand new hard drive in Windows or macOS?

Before you can access a new or formatted drive in your operating system, you need to initialize it first and then create a partition on the drive. A partition defines an area of the drive to use for storing data. The partition uses a file system (for example, ex-FAT, NTFS, and so on).

Initialize a drive

Note: You typically only need to initialize a drive if the drive is new. If you cannot find an uninitialized drive in Disk Management, skip the following steps and try to partition your device.

  1. Press the Windows key + R, type compmgmt.msc, and click Run to open Computer Management.
  2. Navigate to Disk Management.
  3. When prompted to, initialize your disk(s). If you are running Windows® 7 or later and are using a drive larger than 2TB, initialize the disk(s) with GPT. If you are running an earlier version of Windows, initialize the disk(s) with MBR.
  4. Click OK.

Create a partition in a drive

Note: The following steps create an NTFS partition that uses the entire drive space. To use a different file system, select a different option in step 6.

  1. Right-click Unallocated or RAW volume, and select New Simple Volume.
  2. In the New Partition Wizard, click Next.
  3. Select Primary partition.
  4. Leave the partition size set to default, and click Next.
  5. Assign a drive letter or leave it set to the default, and click Next.
  6. Enter the following settings to format the partition:
  • In the File System field, enter NTFS.
  • Set the Allocation unit size to Default.
  • In the Volume label field, enter <your name/reference>.
  • Select the Perform a quick format check box.
  • Clear the Enable file and folder compression check box.
  1. Click Next > Finish.

The new drive should appear in Windows Explorer.

Mac OS

Before you can access a new or formatted drive in your operating system, you need to initialize it first and then create a partition on the drive. A partition defines an area of the drive to use for storing data. The partition uses a file system (for example, HFS+, ex-FAT, NTFS, and so on).

Initialize a drive

Mac OSX detects a drive that needs to be initialized and automatically prompts you to initialize the drive. If you are prompted to initialize the drive, click Initialize. If you are not prompted to initialize the drive and you cannot find the drive in Finder, you will need to create a partition on the drive.

Create a partition on a drive

Note: The following steps create an HFS+ (Mac OS Extended (Journaled)) partition that uses the entire drive space.

To create a partition on a new drive, complete the following:

  1. Open Finder.
  2. Navigate to Applications and click Utilities.
  3. Open Disk Utility.
  4. Select the new drive and click the Partition tab.
  5. Click Options and verify that it is set to GUID Partition Table.
  6. Enter a name for the partition.
  7. Click Partition.

The drive should now be accessible in Finder.

This FAQ applies to these products: M2E1BMU31C S2510BMU33 S2510BPU33 S2510BPU337 S2510BU33PW S251BMU313 S251BPU313 S251BPU31C3 S251BRU31C3 S251BRU33 S251BU31315 S251BU31C3CB S251BU31REMD S251SMU33EP S252BU313R S3510BMU33 S3510SMU33 S351BMU33ET S351BU313 S3520BU33ER S352BU313R S352BU33RER S3540BU33E SAT2510BU32 SATDOCK2REU3 SATDOCK4U3RE SATDOCK5U3ER SATDOCKU3S SATDUP11 SATDUP11IMG SATERASER4 SATSASDUPE11 SDOCK1EU3P SDOCK1EU3P2 SDOCK2U313 SDOCK2U313R SDOCK2U33 SDOCK2U33EB SDOCK2U33RE SDOCK2U33V SDOCK4U313 SDOCK4U33 SDOCKU313 SDOCKU313E SDOCKU33BV SDOCKU33EBV SDOCKU33EF SLSODDU33B SM21BMU31C3 SM21BMU31CI3 SM22BU31C3R SM2NGFFMBU33 SMS1BMU313 SU2DUPERA11 UNI251BMU33 UNIDOCKU33 USBDUP12 USBDUP15 USBDUPE115 USBDUPE17