Hi, David. I have been able to duplicate the problem with two other drives; one WD SATA mechanical drive and a second Samsung SSD. It really looks like an incompatibility between the USB3SSATAIDE and the new system. I have tried moving from the chassis-top USB port to another on the rear. No change.
The ‘working’ system is a Linux machine running Ubuntu 18.04 (yes, older, which is why I’m moving to another box). It is based on an ASUS Z87 motherboard. 32 GB of memory. i7 4.2GHz CPU.
The problem system is running Ubuntu 24.04. It uses an Asrock X870 Pro RS motherboard. 96 GB of memory. AMD Ryzen 9 9900X (24-core).
Here is an extract from /var/log/syslog that shows the low-level issues:
2026-01-14T13:53:53.461431-05:00 thelio kernel: usb 2-3: new SuperSpeed USB device number 18 using xhci_hcd
2026-01-14T13:53:53.474424-05:00 thelio kernel: usb 2-3: New USB device found, idVendor=1f75, idProduct=0611, bcdDevice= 0.06
2026-01-14T13:53:53.474446-05:00 thelio kernel: usb 2-3: New USB device strings: Mfr=4, Product=5, SerialNumber=6
2026-01-14T13:53:53.474447-05:00 thelio kernel: usb 2-3: SerialNumber: 20210911
2026-01-14T13:53:53.495371-05:00 thelio mtp-probe: checking bus 2, device 18: "/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3"
2026-01-14T13:53:53.495489-05:00 thelio mtp-probe: bus: 2, device: 18 was not an MTP device
2026-01-14T13:53:53.503378-05:00 thelio kernel: usb-storage 2-3:1.0: USB Mass Storage device detected
2026-01-14T13:53:53.503384-05:00 thelio kernel: scsi host9: usb-storage 2-3:1.0
2026-01-14T13:53:53.504366-05:00 thelio kernel: usbcore: registered new interface driver usb-storage
2026-01-14T13:53:53.505363-05:00 thelio kernel: usbcore: registered new interface driver uas
2026-01-14T13:53:53.507230-05:00 thelio mtp-probe: checking bus 2, device 18: "/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3"
2026-01-14T13:53:53.507290-05:00 thelio mtp-probe: bus: 2, device: 18 was not an MTP device
2026-01-14T13:53:54.556408-05:00 thelio kernel: scsi host9: scsi scan: INQUIRY result too short (5), using 36
2026-01-14T13:53:54.556429-05:00 thelio kernel: scsi 9:0:0:0: Direct-Access Samsung SSD 870 EVO 1TB PQ: 0 ANSI: 0
2026-01-14T13:53:54.556435-05:00 thelio kernel: sd 9:0:0:0: Attached scsi generic sg2 type 0
2026-01-14T13:53:54.561383-05:00 thelio kernel: sd 9:0:0:0: [sdc] 1953525168 512-byte logical blocks: (1.00 TB/932 GiB)
2026-01-14T13:53:54.562370-05:00 thelio kernel: sd 9:0:0:0: [sdc] Write Protect is off
2026-01-14T13:53:54.562372-05:00 thelio kernel: sd 9:0:0:0: [sdc] Mode Sense: 3b 00 00 00
2026-01-14T13:53:54.563370-05:00 thelio kernel: sd 9:0:0:0: [sdc] No Caching mode page found
2026-01-14T13:53:54.563374-05:00 thelio kernel: sd 9:0:0:0: [sdc] Assuming drive cache: write through
2026-01-14T13:53:54.600374-05:00 thelio kernel: sdc: sdc1
2026-01-14T13:53:54.600384-05:00 thelio kernel: sd 9:0:0:0: [sdc] Attached SCSI disk
2026-01-14T13:53:54.629592-05:00 thelio (udev-worker)[1883140]: sdc: /etc/udev/rules.d/60-ssd-scheduler.rules:1 Failed to write ATTR{/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3/2-3:1.0/host9/target9:0:0/9:0:0:0/block/sdc/queue/scheduler}, ignoring: Invalid argument
2026-01-14T13:53:54.637242-05:00 thelio udisksd[1180]: Error probing device: Error sending ATA command IDENTIFY DEVICE to '/dev/sdc': Unexpected sense data returned:#0120000: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................#0120010: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................#012 (g-io-error-quark, 0)
2026-01-14T13:53:54.643610-05:00 thelio dbus-daemon[1145]: [system] Activating service name='org.kde.kded.smart' requested by ':1.99' (uid=600 pid=2879 comm="/usr/bin/kded5" label="unconfined") (using servicehelper)
2026-01-14T13:53:54.651303-05:00 thelio dbus-daemon[1145]: [system] Successfully activated service 'org.kde.kded.smart'
2026-01-14T13:53:54.673219-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:36:5: Unable to assign [undefined] to bool
2026-01-14T13:53:54.673329-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:35:5: Unable to assign [undefined] to bool
2026-01-14T13:53:54.851222-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:53:54.851325-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:53:54.851443-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:53:54.851473-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:53:54.851488-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:53:54.851587-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:53:58.158932-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:53:58.159134-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:53:58.159236-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:53:58.159265-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:53:58.159279-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:53:58.159426-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:54:19.869402-05:00 thelio kded5[2879]: kf.auth: "Did not receive a reply. Possible causes include: the remote application did not send a reply, the message bus security policy blocked the reply, the reply timeout expired, or the network connection was broken."
2026-01-14T13:54:27.869767-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:174:5: Unable to assign [undefined] to QString
2026-01-14T13:54:27.871317-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:54:27.871374-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:54:27.871472-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:54:27.871613-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:54:27.871636-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:54:27.871747-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:54:36.869515-05:00 thelio plasmashell[2942]: file:///usr/lib/x86_64-linux-gnu/qt5/qml/org/kde/plasma/extras/ExpandableListItem.qml:508:21: QML Label: Binding loop detected for property "verticalAlignment"
2026-01-14T13:54:57.924408-05:00 thelio kernel: usb 2-3: reset SuperSpeed USB device number 18 using xhci_hcd
2026-01-14T13:55:01.901446-05:00 thelio CRON[1883449]: (root) CMD (command -v debian-sa1 > /dev/null && debian-sa1 1 1)
2026-01-14T13:55:59.361418-05:00 thelio kernel: usb 2-3: reset SuperSpeed USB device number 18 using xhci_hcd
2026-01-14T13:55:59.397383-05:00 thelio kernel: EXT4-fs (sdc1): mounted filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233 r/w with ordered data mode. Quota mode: none.
2026-01-14T13:55:59.405831-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.kscreen/contents/ui/InhibitionHint.qml:27:5: QML Label: Binding loop detected for property "verticalAlignment"
2026-01-14T13:55:59.406502-05:00 thelio udisksd[1180]: Mounted /dev/sdc1 at /media/hirsch/6fabe566-3ae9-43fc-ae38-623e48ace233 on behalf of uid 600
2026-01-14T13:56:29.402269-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:56:29.402650-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:56:29.402808-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:56:29.402851-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:56:29.402870-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:56:32.059382-05:00 thelio kernel: EXT4-fs (sdc1): unmounting filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233.
2026-01-14T13:56:29.403015-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:56:32.060118-05:00 thelio systemd[1]: media-hirsch-6fabe566\x2d3ae9\x2d43fc\x2dae38\x2d623e48ace233.mount: Deactivated successfully.
2026-01-14T13:56:32.061423-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:56:32.061449-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:56:32.061512-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:56:32.070917-05:00 thelio udisksd[1180]: Cleaning up mount point /media/hirsch/6fabe566-3ae9-43fc-ae38-623e48ace233 (device 8:33 is not mounted)
2026-01-14T13:56:32.074924-05:00 thelio udisksd[1180]: Unmounted /dev/sdc1 on behalf of uid 600
2026-01-14T13:56:32.101396-05:00 thelio udisksd[1180]: Successfully sent SCSI command SYNCHRONIZE CACHE to /dev/sdc
2026-01-14T13:56:32.101447-05:00 thelio udisksd[1180]: Successfully sent SCSI command START STOP UNIT to /dev/sdc
2026-01-14T13:56:32.109902-05:00 thelio plasmashell[2942]: file:///usr/lib/x86_64-linux-gnu/qt5/qml/org/kde/plasma/extras/ExpandableListItem.qml:291: TypeError: Cannot read property 'enabled' of null
2026-01-14T13:56:32.111896-05:00 thelio plasmashell[2942]: file:///usr/lib/x86_64-linux-gnu/qt5/qml/org/kde/plasma/extras/PlaceholderMessage.qml:238:5: QML Heading: Binding loop detected for property "verticalAlignment"
2026-01-14T13:56:32.169571-05:00 thelio udisksd[1180]: Powered off /dev/sdc - successfully wrote to sysfs path /sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3/remove
2026-01-14T13:56:32.170374-05:00 thelio kernel: usb 2-3: USB disconnect, device number 18
2026-01-14T13:56:50.660406-05:00 thelio kernel: EXT4-fs (sdb1): unmounting filesystem d67b8d4d-8099-40d3-930b-d93bdf71c130.
2026-01-14T13:56:50.660399-05:00 thelio udisksd[1180]: Cleaning up mount point /media/hirsch/d67b8d4d-8099-40d3-930b-d93bdf71c130 (device 8:17 is not mounted)
2026-01-14T13:56:50.660711-05:00 thelio systemd[1]: media-hirsch-d67b8d4d\x2d8099\x2d40d3\x2d930b\x2dd93bdf71c130.mount: Deactivated successfully.
2026-01-14T13:57:12.557464-05:00 thelio kernel: usb 2-3: new SuperSpeed USB device number 19 using xhci_hcd
2026-01-14T13:57:12.571407-05:00 thelio kernel: usb 2-3: New USB device found, idVendor=1f75, idProduct=0611, bcdDevice= 0.06
2026-01-14T13:57:12.571430-05:00 thelio kernel: usb 2-3: New USB device strings: Mfr=4, Product=5, SerialNumber=6
2026-01-14T13:57:12.571433-05:00 thelio kernel: usb 2-3: SerialNumber: 20210911
2026-01-14T13:57:12.589380-05:00 thelio kernel: usb-storage 2-3:1.0: USB Mass Storage device detected
2026-01-14T13:57:12.589383-05:00 thelio kernel: scsi host9: usb-storage 2-3:1.0
2026-01-14T13:57:12.592255-05:00 thelio mtp-probe: checking bus 2, device 19: "/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3"
2026-01-14T13:57:12.592399-05:00 thelio mtp-probe: bus: 2, device: 19 was not an MTP device
2026-01-14T13:57:12.598111-05:00 thelio mtp-probe: checking bus 2, device 19: "/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3"
2026-01-14T13:57:12.598328-05:00 thelio mtp-probe: bus: 2, device: 19 was not an MTP device
2026-01-14T13:57:13.596418-05:00 thelio kernel: scsi host9: scsi scan: INQUIRY result too short (5), using 36
2026-01-14T13:57:13.596481-05:00 thelio kernel: scsi 9:0:0:0: Direct-Access Samsung SSD 870 EVO 1TB PQ: 0 ANSI: 0
2026-01-14T13:57:13.596506-05:00 thelio kernel: sd 9:0:0:0: Attached scsi generic sg2 type 0
2026-01-14T13:57:13.601372-05:00 thelio kernel: sd 9:0:0:0: [sdc] 1953525168 512-byte logical blocks: (1.00 TB/932 GiB)
2026-01-14T13:57:13.602368-05:00 thelio kernel: sd 9:0:0:0: [sdc] Write Protect is off
2026-01-14T13:57:13.602370-05:00 thelio kernel: sd 9:0:0:0: [sdc] Mode Sense: 3b 00 00 00
2026-01-14T13:57:13.603364-05:00 thelio kernel: sd 9:0:0:0: [sdc] No Caching mode page found
2026-01-14T13:57:13.603365-05:00 thelio kernel: sd 9:0:0:0: [sdc] Assuming drive cache: write through
2026-01-14T13:57:13.633385-05:00 thelio kernel: sdc: sdc1
2026-01-14T13:57:13.633394-05:00 thelio kernel: sd 9:0:0:0: [sdc] Attached SCSI disk
2026-01-14T13:57:13.664641-05:00 thelio (udev-worker)[1884029]: sdc: /etc/udev/rules.d/60-ssd-scheduler.rules:1 Failed to write ATTR{/sys/devices/pci0000:00/0000:00:02.1/0000:02:00.0/0000:03:0c.0/0000:0b:00.0/usb2/2-3/2-3:1.0/host9/target9:0:0/9:0:0:0/block/sdc/queue/scheduler}, ignoring: Invalid argument
2026-01-14T13:57:13.670816-05:00 thelio udisksd[1180]: Error probing device: Error sending ATA command IDENTIFY DEVICE to '/dev/sdc': Unexpected sense data returned:#0120000: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................#0120010: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................#012 (g-io-error-quark, 0)
2026-01-14T13:57:13.676044-05:00 thelio dbus-daemon[1145]: [system] Activating service name='org.kde.kded.smart' requested by ':1.99' (uid=600 pid=2879 comm="/usr/bin/kded5" label="unconfined") (using servicehelper)
2026-01-14T13:57:13.684171-05:00 thelio dbus-daemon[1145]: [system] Successfully activated service 'org.kde.kded.smart'
2026-01-14T13:57:13.702347-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:36:5: Unable to assign [undefined] to bool
2026-01-14T13:57:13.702452-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:35:5: Unable to assign [undefined] to bool
2026-01-14T13:57:13.882026-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:57:13.882062-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:57:13.882157-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:57:13.882222-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:57:13.882236-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:57:13.882342-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:57:18.073006-05:00 thelio kwin_x11[2880]: kwin_core: XCB error: 152 (BadDamage), sequence: 45477, resource id: 32913657, major code: 143 (DAMAGE), minor code: 3 (Subtract)
2026-01-14T13:57:38.867641-05:00 thelio kded5[2879]: kf.auth: "Did not receive a reply. Possible causes include: the remote application did not send a reply, the message bus security policy blocked the reply, the reply timeout expired, or the network connection was broken."
2026-01-14T13:57:42.869283-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.plasma.devicenotifier/contents/ui/DeviceItem.qml:174:5: Unable to assign [undefined] to QString
2026-01-14T13:57:42.870874-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:181:21 depends on non-NOTIFYable properties:
2026-01-14T13:57:42.870915-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:57:42.871021-05:00 thelio plasmashell[2942]: message repeated 7 times: [ QAction::priority]
2026-01-14T13:57:42.871131-05:00 thelio plasmashell[2942]: QQmlExpression: Expression file:///usr/share/plasma/plasmoids/org.kde.plasma.private.systemtray/contents/ui/ExpandedRepresentation.qml:82:17 depends on non-NOTIFYable properties:
2026-01-14T13:57:42.871145-05:00 thelio plasmashell[2942]: QAction::priority
2026-01-14T13:58:14.532416-05:00 thelio kernel: usb 2-3: reset SuperSpeed USB device number 19 using xhci_hcd
2026-01-14T13:59:15.973430-05:00 thelio kernel: usb 2-3: reset SuperSpeed USB device number 19 using xhci_hcd
2026-01-14T13:59:16.013393-05:00 thelio kernel: EXT4-fs (sdc1): mounted filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233 r/w with ordered data mode. Quota mode: none.
2026-01-14T13:59:16.013412-05:00 thelio kernel: EXT4-fs (sdc1): unmounting filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233.
2026-01-14T13:57:42.871255-05:00 thelio plasmashell[2942]: message repeated 8 times: [ QAction::priority]
2026-01-14T13:59:16.013943-05:00 thelio udisksd[1180]: Error removing directory /media/hirsch/6fabe566-3ae9-43fc-ae38-623e48ace233: No such file or directory
2026-01-14T13:59:16.015096-05:00 thelio plasmashell[2942]: file:///usr/share/plasma/plasmoids/org.kde.kscreen/contents/ui/InhibitionHint.qml:27:5: QML Label: Binding loop detected for property "verticalAlignment"
2026-01-14T13:59:16.022094-05:00 thelio udisksd[1180]: Mounted /dev/sdc1 at /media/hirsch/6fabe566-3ae9-43fc-ae38-623e48ace233 on behalf of uid 600
2026-01-14T13:59:16.022367-05:00 thelio kernel: EXT4-fs (sdc1): mounted filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233 r/w with ordered data mode. Quota mode: none.
2026-01-14T14:00:01.585844-05:00 thelio systemd[1]: Starting sysstat-collect.service - system activity accounting tool...
2026-01-14T14:00:01.589354-05:00 thelio systemd[1]: sysstat-collect.service: Deactivated successfully.
2026-01-14T14:00:01.589483-05:00 thelio systemd[1]: Finished sysstat-collect.service - system activity accounting tool.
2026-01-14T14:00:17.994831-05:00 thelio systemd[1]: mnt.mount: Deactivated successfully.
2026-01-14T14:00:27.124391-05:00 thelio kernel: usb 2-3: USB disconnect, device number 19
2026-01-14T14:00:27.124411-05:00 thelio kernel: EXT4-fs (sdc1): shut down requested (2)
2026-01-14T14:00:27.124412-05:00 thelio kernel: Aborting journal on device sdc1-8.
2026-01-14T14:00:27.124413-05:00 thelio kernel: device offline error, dev sdc, sector 973342720 op 0x1:(WRITE) flags 0x9800 phys_seg 1 prio class 2
2026-01-14T14:00:27.124414-05:00 thelio kernel: Buffer I/O error on dev sdc1, logical block 121667584, lost sync page write
2026-01-14T14:00:27.124414-05:00 thelio kernel: JBD2: I/O error when updating journal superblock for sdc1-8.
2026-01-14T14:00:27.286124-05:00 thelio udisksd[1180]: Cleaning up mount point /media/hirsch/6fabe566-3ae9-43fc-ae38-623e48ace233 (device 8:33 no longer exists)
2026-01-14T14:00:27.290351-05:00 thelio systemd[1]: media-hirsch-6fabe566\x2d3ae9\x2d43fc\x2dae38\x2d623e48ace233.mount: Deactivated successfully.
2026-01-14T14:00:27.290375-05:00 thelio kernel: EXT4-fs (sdc1): unmounting filesystem 6fabe566-3ae9-43fc-ae38-623e48ace233.