Hello there,
I have a laptop that I use for both work and gaming. It is a pretty decent machine with an Intel i7 processor; 16GB of RAM; and an NVIDIA GTX 1660 Ti graphics card. The laptop itself has an HDMI port and a USB-C port that supports DisplayPort.
I have recently been considering expanding my screen real estate by adding multiple external monitors. My goal is to set up two additional monitors for a total of three screens; including the laptops built in display.
This setup is mainly for productivity purposes; such as multitasking between different applications and occasionally for gaming.
I have read that using a docking station or a USB-C hub can simplify connecting multiple monitors. Could someone recommend a StarTech product that would be suitable for this purpose?
Ideally; I would like a solution that can support two 1080p monitors in addition to my laptop screen.
How does using a docking station or hub affect performance; especially when it comes to gaming or graphics intensive tasks?
My primary concern is ensuring that there is no noticeable lag or drop in quality when using external monitors.
What kind of cables and adapters would I need to ensure everything works smoothly? For instance; do I need specific types of HDMI or DisplayPort cables; or are there any StarTech adapters that you would recommend? ![]()
Also, I have gone through this post; https://community.startech.com/t/how-to-setup-an-extended-display-in-windows-golang/ which definitely helped me out a lot.
Are there any other tips or considerations I should keep in mind when setting up multiple monitors with a laptop? ![]()
Thanks in advance for your help and assistance. ![]()