Does the 1394 PCI Firewire card work OK with Win 11?
(the PEX1394B3LP)
Does the 1394 PCI Firewire card work OK with Win 11?
(the PEX1394B3LP)
Hello AS63,
I hope you’re well.
Fortunately, our PEX1394B3LP PCIe card does support Windows 11:
However, you may need to load the generic Firewire driver stack from Microsoft into Windows as this driver stack is often not included in recent Windows builds. We have an FAQ on how to do this in Windows 10, and the steps ought to be the same on your Windows 11 system: Install the Firewire 1394 Legacy Driver in Windows 10 | StarTech.com
How do I install the Firewire 1394 Legacy Driver in Windows 10?
Download the Microsoft Firewire 1394 Legacy Driver Installer
Double-click to run the 1394_OHCI_LegacyDriver.msi file. This will extract the drivers to: C:\Program Files (x86)\1394 OHCI Compliant Host Controller (Legacy)\
Open the folder: C:\Program Files (x86)\1394 OHCI Compliant Host Controller (Legacy)\X64_driver\
Right-click on Legacy1394.inf and choose Install to install the drivers
Press the Windows Key + R
Type devmgmt.msc
Click OK
In Device Manager, expand IEEE 1394 Bus Host Controllers
Right-click on 1394 OHCI Compliant Host Controller
Click Update Driver Software
Click Browse my computer for driver software
Click Let me pick from a list of device drivers on my computer
Click 1394 OHCI Compliant Host Controller (Legacy)
Click Next
(When Windows has finished installing the driver) click Close
All the best,
Brent