diskmgmt.msc sees the USB3S2SAT3CB USB 3.0 to 2.5" SATA cable as a ASMT2235 USB Device and with a 4TB drive with existing partition it works. I can click on the drive in windows and see the data. However with a 1TB drive split into two partitions it shows as ‘No Media’ and when I click on the drive icon in Windows it pops up “please insert a disk into USB Drive”
Both drives are WD Blue SATA III standard 2.5" SSD.
Now the reason I bought the adaptor is the 1TB drive had the mechanical L get nicked so it was not locking in place for electrical contact. I was hoping the adaptor having bridging support between power/data connectors would give it a mechanical support for making electrical contact.
But it did not work so I need to find out if it is just the firmware- is it supporting drives with multiple partitions?