I’m trying to read a SSD drive with the M.2 to U.2 Adapter - For M.2 PCIe NVMe SSDs - PCIe M.2 Drive to 2.5" U.2 (SFF-8639) Host Adapter - M2 SSD Converter, Red, but in my laptop in Windows 10 64 bits, the drive showed up gray out
Hello @socorrorosas. We appreciate you taking the time to post on our Community forum.
It appears you are using the U2M2E125 which is used to connect a M.2 PCIe NVMe SSD to a U.2 (SFF-8639) host. In addition, the USB3S2SAT3CB is used to connect a standard 2.5" SSD or HDD. Unfortunately, the USB3S2SAT3CB and U2M2E125 will not work in conjunction since these devices support different hard drive connections.
We would like gather information about your setup and look into a possible solution. Please reply here with the specific make/model of the drive you’re trying to connect, so we can help further.
Thank you in advance, and we look forward to hearing from you!