To use the S2510BU3ISO to load ISO images, the drive must have the following parameters:
If the enclosure is not formatted with these parameters, it will not lock on to an ISO (located in an _iso folder) and will only function as an external mass storage device.