Meaning of the LED indicators on the SM22BU31C3R


Two FIKWOT FN203 (M.2 2280 SATA SSD) drives in an SM22BU31C3R.

The SSD1 and SSD2 LEDs blink white once per second, and the SSD1 LED is also solid red.

Why?


Thank you for your help.

Chat Celte

 

Hello @ChatCelte and thank you for your interest in our Community.

From the description that you are providing, it would seem like your SSD1 has failed. Were you using them in JBOD, RAID 0/1 or SPAN?

→ If you were using them in RAID, then the next step would be to replace SSD1 with another comparable drive and let the enclosure rebuild the array.

→ If you simply had them in JBOD, then you are free to replace the drive with any other compatible drive as well as test the SDD1 in another enclosure or internally in a computer to confirm the defective status.

For your information, the LED details can be found in our instruction manual on P.2:

Have a great day and good luck with your drive.

Emmanuel B.
StarTech.com Support


complete setup : Two FIKWOT FN203 (M.2 2280 SATA SSD) drives in an SM22BU31C3R in RAID 1.

The SSD2 LED blink white once per second, the SSD1 LED blink white once per second and also solid red.

But now, everything is as before. I assume SSD1 was being rebuilt?

Thank you for your help.

Chat Celte

Hello @ChatCelte ,

It is possible. Or there was a temporary read error.

If the LEDs are no longer showing any errors, you should be alright. But if SSD1 goes back to blinking red again at some later time, I would recommend verifying and potentially replacing that drive.

Have a great day!

Emmanuel B.
StarTech.com Support