I have the Startech SDOCKU33EF, to which I connect a 3.5" drive. Having a built in fan into the dock is fantastic, but I find out that it’s very noisy, regardless if the fan speed (PWM I guees) is to 100% or less.
Could be possible to replace this fan with some very silent one, like Noctua? I just can’t sleep with this and it’s noticeable in the office that I have “something” running. I would like to have really some help even if I have to perform some unauthorized modification. I really need a silent dock BUT WITH SOME COOLING.