4PORT-8K-HDMI-SWITCH - No automatic switching on of the sound bar or TV when sources are switched ON on HDMI 2 to 4

Hello @Albrator,

We do have another 4 port HDMI video switch that supports CEC, this would be our VS421HD20. However this switch supports a maximum resolution and refresh rate of 4K at 60Hz, rather than 8K 60Hz or 4K 120Hz like 4PORT-8K-HDMI-SWITCH does.

Lukas T