Need to Digitize S-VHS VCR output: S-video or composite, or, via Extron IN1502, VGA

I have a good working Panasonic AG-7650HP S-VHS Hi-Fi Player with S-VHS output and the Faroudja circuitry cleans up old tapes decently. I also have, but have not yet tried using an Extron IN1502 S-Video to VGA video scaler to see if that helps or not. I question feeding my signal into a $20 converter to get to digital. Suggestions? I have several hundred tapes to process. I have a separate monitor output, so that is not an issue.

USB-C would be preferable. I can re-sync the audio in software if path delays are an issue.

In case it makes a difference to anyone, the several hundred I want to digitize are the select few I expect will be worth digitizing out of a total collection of a couple thousand locally recorded tapes. The total quantity of commercially produced tapes in the larger group is probably under a dozen and of no interest, thus copy protection or a need to defeat it is not an issue at all. 99% I recorded myself. Largest category groups are family and church services where I did the A/V work for years.