I have multiple SATA HDDs I need to access (Data only, no Videos) so purchased the 4 Bay USB Dock SDOCK4U33E. I had hoped that with it having USB 3.1 output that it would connect to a Macbook 2024 via the USB C and allow me to see all of the HDDs on the Mac OS Finder. The connection is by the Apple USB C to USB Adapter. I have also tried an Avent AMHBCPD19 5-port USB Type-C with no success.
Sadly I can only have one HDD switched on at a time in the 4 bay dock and see it. As soon as I turn on a second HDD, Mac OS Finder loses sight of all of the HDDs.
Is there a connector I can use to see all of the HDDs at the same time or have I purchased the wrong product? Is there a software download I need ?
Thanks for any help