Hi David,
Our IT has been researching and we are waiting on a new MS driver to solve the issue. The driver used for the USB32HD2 does not release the memory and eventually freezes.
- How many USB32HD2 units do you have in total? Including units that do not have this issue. I am not sure, our associates are spread out and I do not have access to those numbers.
- You mentioned that several associates are experiencing their monitors freezing up intermittently however only 1 was noted above.
- Are multiple associates using the same USB32HD2? No
- How many USB32HD2 units are experiencing the issue? We have 10 that reported and the rest are using the workaround until a driver is available. Rather than unplugging the adapter, kill the process(es): “Windows Driver Foundation” via the task manager that’s accessible by right-clicking the taskbar and choosing “Task Manager”.
- Have the USB32HD2 worked correctly for you before, or has this issue persisted since the beginning? Worked before a MS update that happened around Nov. 2023.
- If the USB32HD2 has worked correctly for you before, did anything change before it stopped. Yes, there was a Windows 11 Pro update in Nov. 2023 and the issue started happening.
- When were the USB32HD2 adapters purchased? Various dates. The latest one I received is Part#1523010521.