USB32HD4: Intermittent Freezing on Two HDMI Ports

Hello,

I’m experiencing an issue with my StarTech.com USB32HD4 4-Port USB 3.0 to HDMI Adapter.

Here’s the problem:

  • Two of the four HDMI ports randomly freeze, displaying a static image.
  • The freezing always occurs on the same two HDMI ports. Either ports 1 and 3 freeze, or ports 2 and 4 freeze. There are no other patterns.
  • This occurs on Windows 11.
  • I’ve tried using different HDMI cables and connecting to different monitors, but the issue persists.
  • Connecting the adapter to a different PC results in the same problem.
  • The issue is temporarily resolved by unplugging and reconnecting the USB 3.0 cable, effectively restarting the adapter.
  • I have the latest device drivers installed, version 24.01.0730.3679.
  • I use this device daily for work, and the issue occurs approximately every two days.
    Has anyone else encountered this issue or have any suggestions for troubleshooting?

Thank you.

Thank you @shane for your interest in our Community.

Display issues like intermittent freezing can often be influenced by how the USB video adapter interacts with your computer’s graphics hardware and system configuration. Before considering any issue on the hardware side, it would be important to first troubleshoot any potential software issue first by ensuring an optimal setup process. To do so, we recommend following these troubleshooting steps:

  1. Disconnect our device and Uninstall the current USB video drivers from your system.
  2. Update your computer’s BIOS/Firmware to the latest version available from your system or motherboard manufacturer.
  3. Update your graphics card drivers directly from the GPU manufacturer’s website (e.g., Intel, AMD, NVIDIA).
  4. Restart your computer to ensure all updates are properly applied.
  5. Download the latest USB video drivers for your adapter from the www.startech.com/USB32HD4.
  6. After downloading, extract the driver files completely.
  7. Right-click on the setup file and select “Run as Administrator” to begin installation. This ensures the installer has the necessary permissions to configure the driver correctly.
  8. When ready, simply reconnect our device to your computer.

Following these steps helps eliminate potential conflicts and ensures the adapter is working with the most stable and compatible system environment.

We appreciate your patience and hope this helps resolve the issue!

Emmanuel B.

Hi @EmmanuelB,

Thank you for your advice. I followed all the steps you provided, including uninstalling the current USB video drivers, updating my computer’s BIOS/Firmware and graphics card drivers, and reinstalling the latest USB video drivers from your website.

I’ve been monitoring the situation for over a month now since implementing your suggestions. Unfortunately, the issue of intermittent freezing on two HDMI ports (1 and 3, or 2 and 4) still persists. The problem now occurs about once or twice a week, and the only temporary solution remains unplugging and reconnecting the USB 3.0 cable.

Any further suggestions would be greatly appreciated.

Thanks, Shane

Hello @shane, I am sorry to hear that the issue persists. At this point, I would recommend you to contact our Technical Support (by chat or phone) while in front of the equipment in question.

We look forward to hearing back from you.

Emmanuel B.

Hi @EmmanuelB, thank you for your help. I will contact technical support as you recommended.