Adapter for WD Scorpio Black 320GB WD3200BEKT 7200RPM 16MB SATA 2.5" Laptop Hard Disk Drive

Can anyone recommend me that which adapter should I use to read

“WD Scorpio Black 320GB WD3200BEKT 7200RPM 16MB SATA 2.5” Laptop Hard Disk Drive"

as an external drive.

Thanks

Arif

Hello @arifakhtar2004 ! Thank you for posting your question.

As that is a SATA drive using the 2.5" form factor with a 9.5mm height, I would recommend the following options:

USB 3.0 - S2510BPU33, S2510BMU33

USB 3.1 - S251BMU313

USB 3.0 (more durable, rugged) - S251BRU33

All of these options include a USB-A cable to connect to your computer. If you prefer connecting via USB-C, an adapter such as our USB31CAADP or cable such as our USB31CUB50CM can be used.

If you have any questions or require any additional assistance, please don’t hesitate to reach out!

Jean