I’ve had my DK31C2DHSPD dock now for several months now. I have three monitors connected to it: 2 monitors connected via the display port connection using Display port to HDMI Cables and 1 connected via the HDMI connection using an HDMI to DVI Dual Link connector.
I keep having constant connection issues-
The monitor on the HDMI output has to be unplugged and plugged back in several times in order to get it to connect. Sometimes it connects with absolutely no issue, but it’s rare. It’s extremely annoying, and it makes no sense as to why it works intermittently but often fails to connect.
The monitors on the display port go blank extremely often for a few seconds during use then turn back on. One sometimes only comes back as a white screen, or they both will come back with fuzzy connections. Sometimes they completely fail to connect without the cable being unplugged and plugged back in.
Today they started a new, annoying behavior: They all go to complete static intermittently and then go black. Then the center (HDMI) screen will turn back on, briefly go to static and then display properly. The two other screens (DP) will then follow and do the same.
It sounds to me like either I have a faulty dock or that there’s a firmware issue. I have no issues whatsoever with my Lenovo laptop when using it with other docking stations through either USB-C ports or using it with just an external monitor on its HDMI connector.
Has anyone had any similar issues? I’ve used StarTech products for years with little to no issues, so I am really surprised at the problems I am having with this dock.