Lukas, thank you. Generic PC hardware running linux that has been configured to output 15 KHz/240p. I want to use the VGA2VID as a media converter to get the video signals on CRTs with composite/svideo inputs.
jeffbrl
5
Related topics
| Topic | Replies | Views | Activity | |
|---|---|---|---|---|
| VGA to HDMI supporting 640x480@60 and 720x400 @70 | 12 | 33845 | March 17, 2022 | |
| VGA2HDU compatibility with 720x400@70 Hz | 4 | 303 | January 30, 2025 | |
| Latency in converting from HDMI->VGA & VGA->PAL | 4 | 171 | September 27, 2024 | |
| My Linux and Mac computers don't "see" the real monitor, can the KVM default be changed? | 5 | 625 | April 12, 2023 | |
| ISSUE with NOTECONS02 Hdmi to VGA adapter | 1 | 282 | July 24, 2023 |