Hello,
I have a StarTech 4xHDD RAID Enclosure (SAT3540U3ER),
I plugged in four Hitachi 4GB Sata3 HDDs (HDS724040ALE640) and configured them for RAID-5, giving a volume capacity of 11GB.
I have noticed recently that the unit has the REBUILD light on and two red RAID lights: +1 and +5. There is no drive warning light.
There is no rebuild going on, the unit goes into sleep mode after some time.
I’m therefore attempting to reset the unit, by following these instructions:
- Turn off the enclosure and remove the drives.
- Power the enclosure back up and set it to RAID 0 by pressing the “Mode” button Press and hold the “Confirm” button on the back of the enclosure next to the ESATA port behind the plastic cover, until it powers off.
- Install the drives.
- Turn the power back on.
Step 1: OK
Step 2: Not OK
- I press the power button. Nothing.
- I press the Mode button and the unit turns itself on, the fan starts to spin up, then, after ~5 seconds, the unit turns itself off again.
- Pressing the Mode button a second time does nothing.
- It’s as if there was some residual power in the unit (the unit is plugged into its PSU and turned on), just enough for a 5-second power-up before it was drained.
Has anyone seen this happen before? The power button doesn’t turn the unit on but the “mode” button does, and only for a few seconds.
Kind regards,
Paul